Layerscape JTAG port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Layerscape JTAG port

Jump to solution
4,497 Views
tom_derks
Contributor I

Hi,

 

When programming layerscape CPU with Code warrior programmer is native JTAG used or is the protocol SWD? I need to know wether JTAG TDI connection is required or not.

 

best regards,

Tom

0 Kudos
Reply
1 Solution
4,477 Views
ufedor
NXP Employee
NXP Employee

Correct.

Only JTAG functions of signals are used.

View solution in original post

0 Kudos
Reply
5 Replies
4,491 Views
tom_derks
Contributor I

ulinkplus_jtag_10pin_swm

Does the codewarrior programmer for layerscape with 10-pin arm debug connector only support JTAG or also SWD? 

0 Kudos
Reply
4,484 Views
ufedor
NXP Employee
NXP Employee

Which processor is in question?

Have you read the processor Design Checklist document?

0 Kudos
Reply
4,481 Views
tom_derks
Contributor I

It is for LS1043A CPU, i see nothing about SWD in checklist/reference manual so i guess it's not supported.

We will just implement the 10-pin JTAG connector.

 

Tags (1)
0 Kudos
Reply
4,478 Views
ufedor
NXP Employee
NXP Employee

Correct.

Only JTAG functions of signals are used.

0 Kudos
Reply
4,493 Views
ufedor
NXP Employee
NXP Employee

You wrote:
> wether JTAG TDI connection is required or not.
The request is not clear. 
TDI is essential JTAG signal. 

0 Kudos
Reply