Layerscape JTAG port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,495件の閲覧回数
tom_derks
Contributor I

Hi,

 

When programming layerscape CPU with Code warrior programmer is native JTAG used or is the protocol SWD? I need to know wether JTAG TDI connection is required or not.

 

best regards,

Tom

0 件の賞賛
返信
1 解決策
4,475件の閲覧回数
ufedor
NXP Employee
NXP Employee

Correct.

Only JTAG functions of signals are used.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,489件の閲覧回数
tom_derks
Contributor I

ulinkplus_jtag_10pin_swm

Does the codewarrior programmer for layerscape with 10-pin arm debug connector only support JTAG or also SWD? 

0 件の賞賛
返信
4,482件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which processor is in question?

Have you read the processor Design Checklist document?

0 件の賞賛
返信
4,479件の閲覧回数
tom_derks
Contributor I

It is for LS1043A CPU, i see nothing about SWD in checklist/reference manual so i guess it's not supported.

We will just implement the 10-pin JTAG connector.

 

タグ(1)
0 件の賞賛
返信
4,476件の閲覧回数
ufedor
NXP Employee
NXP Employee

Correct.

Only JTAG functions of signals are used.

0 件の賞賛
返信
4,491件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:
> wether JTAG TDI connection is required or not.
The request is not clear. 
TDI is essential JTAG signal. 

0 件の賞賛
返信