LX2160: Adding new flash device to Code warrior flash programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LX2160: Adding new flash device to Code warrior flash programmer

1,598件の閲覧回数
rams
Contributor I

Does CW flash programmer support MX66UM1G45G flash device?

 I tried using the default flash device MT35XU512ABA supported for the Lx2160A RDB.  I was able to program once. But it does not work after programming it second time.

I referred the documentation to add a new flash device.

https://community.nxp.com/t5/Layerscape-Knowledge-Base/LX2160ARDB-How-to-configure-a-new-flash-devic...

 

Is that possible to add MX66UM1G45G  similar way?  Can you give details on choosing the closest device file which can be used to create configuration for the new device?

 

Thanks

タグ(1)
0 件の賞賛
返信
1 返信

1,594件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:

> Is that possible to add MX66UM1G45G similar way?

Yes.

> Can you give details on choosing the closest device file

> which can be used to create configuration for the new device?

c:\Freescale\CW4NET_v2020.06\CW_ARMv8\Config\flash\devices\MT35XU512ABA.xml

0 件の賞賛
返信