LX2160: Adding new flash device to Code warrior flash programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160: Adding new flash device to Code warrior flash programmer

1,607 Views
rams
Contributor I

Does CW flash programmer support MX66UM1G45G flash device?

 I tried using the default flash device MT35XU512ABA supported for the Lx2160A RDB.  I was able to program once. But it does not work after programming it second time.

I referred the documentation to add a new flash device.

https://community.nxp.com/t5/Layerscape-Knowledge-Base/LX2160ARDB-How-to-configure-a-new-flash-devic...

 

Is that possible to add MX66UM1G45G  similar way?  Can you give details on choosing the closest device file which can be used to create configuration for the new device?

 

Thanks

Tags (1)
0 Kudos
Reply
1 Reply

1,603 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> Is that possible to add MX66UM1G45G similar way?

Yes.

> Can you give details on choosing the closest device file

> which can be used to create configuration for the new device?

c:\Freescale\CW4NET_v2020.06\CW_ARMv8\Config\flash\devices\MT35XU512ABA.xml

0 Kudos
Reply