LS1046A debug connection failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A debug connection failure

2,234件の閲覧回数
StephenLi
Contributor I

Hi, there is custom board with LS1046A (1.8GHz) with discrete ddr4 (32bit bus, 2100MT/s)

it could go through qcvs ddr validation tool for parameters fine tune. 

it is updated  ddr parameters in duplicated LS1046A_FRWY target configuration 

initialization file  and set use_safe_rcw true  with modified RCW 

the connection is not successful, I dnot find any error in the log. 

please help to advise what is setting wrong caused the issue.

should  it use LS1046A_FRWY or LS1046A_RDB?

0 件の賞賛
返信
1 返信

2,185件の閲覧回数
khushbur
NXP TechSupport
NXP TechSupport

Hi

You can use LS1046A_FRWY as a referance but you need to modify it according to your custom board.

On your board do you have some DIP SW settings for hard-coded RCW? If yes..can you set up them?

Can you please share application which you are debugging?

Thanks

Khushbu

0 件の賞賛
返信