LS1046A TA_TMP_DETECT_B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A TA_TMP_DETECT_B

ソリューションへジャンプ
1,931件の閲覧回数
sinu52
Contributor II

Hello,

I have a question about document AN5252 QorIQ LS1046A Design checklist.

On page 27 it states that both TA_BB_TMP_DETECT_B and TA_TMP_DETECT_B, when used they should be pulled down with a 1K resistor. In all reference designs of LS1046A and LS1028 the signals are pulled up.

Since these signals are LOW active. Wont this trigger a tamper right away?

Kind regards,

Remco

0 件の賞賛
返信
1 解決策
1,925件の閲覧回数
ufedor
NXP Employee
NXP Employee

The AN5252 means the following connection circuit:Tamper.jpg

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,926件の閲覧回数
ufedor
NXP Employee
NXP Employee

The AN5252 means the following connection circuit:Tamper.jpg

0 件の賞賛
返信