LS1046A TA_TMP_DETECT_B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A TA_TMP_DETECT_B

跳至解决方案
1,933 次查看
sinu52
Contributor II

Hello,

I have a question about document AN5252 QorIQ LS1046A Design checklist.

On page 27 it states that both TA_BB_TMP_DETECT_B and TA_TMP_DETECT_B, when used they should be pulled down with a 1K resistor. In all reference designs of LS1046A and LS1028 the signals are pulled up.

Since these signals are LOW active. Wont this trigger a tamper right away?

Kind regards,

Remco

0 项奖励
回复
1 解答
1,927 次查看
ufedor
NXP Employee
NXP Employee

The AN5252 means the following connection circuit:Tamper.jpg

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,928 次查看
ufedor
NXP Employee
NXP Employee

The AN5252 means the following connection circuit:Tamper.jpg

0 项奖励
回复