LS1046A TA_TMP_DETECT_B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A TA_TMP_DETECT_B

Jump to solution
1,954 Views
sinu52
Contributor II

Hello,

I have a question about document AN5252 QorIQ LS1046A Design checklist.

On page 27 it states that both TA_BB_TMP_DETECT_B and TA_TMP_DETECT_B, when used they should be pulled down with a 1K resistor. In all reference designs of LS1046A and LS1028 the signals are pulled up.

Since these signals are LOW active. Wont this trigger a tamper right away?

Kind regards,

Remco

0 Kudos
Reply
1 Solution
1,948 Views
ufedor
NXP Employee
NXP Employee

The AN5252 means the following connection circuit:Tamper.jpg

View solution in original post

0 Kudos
Reply
1 Reply
1,949 Views
ufedor
NXP Employee
NXP Employee

The AN5252 means the following connection circuit:Tamper.jpg

0 Kudos
Reply