LS1046A: Bare-Metal header files and driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A: Bare-Metal header files and driver

ソリューションへジャンプ
2,927件の閲覧回数
tomhohenstein
Contributor I

Hello,

I would like to do some bare-metal development on a custom LS1046A board. I know from other processors that there are often header files containing at least definitions for register addresses or even complete drivers which serve as an hardware abstraction layer.

Does NXP provide any of this for the LS1046A processor to support bare-metal developement?

I've searched the LSDK, the QorIQ SDK and in CodeWarrior but did not find anything.

Any help would be much appreciated!

タグ(2)
0 件の賞賛
返信
1 解決策
2,709件の閲覧回数
Pavel
NXP Employee
NXP Employee

There are program examples in CW4NET for ARM. These examples contain .h files for eSDHC and qSPI. Use the following path:

C:\Freescale\CW4NET_v2018.01\CW_ARMv8\ARMv8\CodeWarrior_Examples

 

There is a few .h file in u-boot source in SDK 2.0-1703 or LSDK.

Use the following path is LSDK:

flexbuild/packages/firmware/u-boot/include

and

use the following path is SDK 2.0-1703:

QorIQ-SDK-V2.0-20160527-yocto/build_ls1046ardb/tmp/work/ls1046ardb-fsl-linux/u-boot-qoriq/2016.09+fslgit-r0/git/include

 

Find the fsl*.h file in these folders.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,710件の閲覧回数
Pavel
NXP Employee
NXP Employee

There are program examples in CW4NET for ARM. These examples contain .h files for eSDHC and qSPI. Use the following path:

C:\Freescale\CW4NET_v2018.01\CW_ARMv8\ARMv8\CodeWarrior_Examples

 

There is a few .h file in u-boot source in SDK 2.0-1703 or LSDK.

Use the following path is LSDK:

flexbuild/packages/firmware/u-boot/include

and

use the following path is SDK 2.0-1703:

QorIQ-SDK-V2.0-20160527-yocto/build_ls1046ardb/tmp/work/ls1046ardb-fsl-linux/u-boot-qoriq/2016.09+fslgit-r0/git/include

 

Find the fsl*.h file in these folders.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,709件の閲覧回数
tomhohenstein
Contributor I

Thank you for your answer even though it is unfortunate that there is no complete bare metal SDK.

0 件の賞賛
返信