Yocto QorIQ SDK v2.0-1806 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto QorIQ SDK v2.0-1806 ?

2,120 Views
nic30
Contributor I

Hello,

I see that there is flexbuild for LSDK v18.06, when there will be Yocto QorIQ SDK v2.0-1806 (for LS2088ardb)?

I have manually updated Yocto SDK 17.12 which can be downloaded from GitHub - qoriq-open-source/yocto-sdk .

Labels (1)
0 Kudos
Reply
2 Replies

1,624 Views
Pavel
NXP Employee
NXP Employee

NXP offers Linux SDK 2.0-1703 BSP for the LS2088ARDB board.

See SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

NXP offers also new Linux BSPO for ARM base processors - LSDK.

This LSDK supports the LS2088ARDB board.

See LSDK documentation:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.06.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,624 Views
nic30
Contributor I

Yes, NXP offers Linux SDK 2.0-1703 but when it gets current update?

0 Kudos
Reply