LS1046 RESET_REQ_B problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 RESET_REQ_B problem

2,896 Views
gaborkocsis
Contributor III

Hello Everybody,

I have faced a weird phenomenon on our custom board based on an LS1046A.

In a CPLD I've implemented a power and reset sequence. I was able to bring up our board, the Linux runs correctly from the onboard eMMC,
BUT,

the LS1046's RESET_REQ_B constantly pulled down. During the reset sequence it goes high then goeas back low
Despite of this everything seems to be OK.

But I don't understand this phenomenon.

Has anybody faced this before?

thanks in advance,

Gabor

0 Kudos
Reply
2 Replies

2,434 Views
flashingsky
Contributor II

I meet the same problem.I'm very puzzled now.

If I used the RESET_REQ_B of LS1046A to trig a power on reset. LS1046A can not bring up.

0 Kudos
Reply

2,651 Views
ufedor
NXP Employee
NXP Employee

Described behaviour means that there is an issue with RCW.

The first point to check is SerDes reference clocks - they should have correct frequencies and should be provided for all PLLs which are not explicitly powered down in the RCW.

In case of further question please provide the processor connection schematics as searchable PDF for inspection along with U-Boot log.

0 Kudos
Reply