LS1046 RESET_REQ_B problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 RESET_REQ_B problem

2,895件の閲覧回数
gaborkocsis
Contributor III

Hello Everybody,

I have faced a weird phenomenon on our custom board based on an LS1046A.

In a CPLD I've implemented a power and reset sequence. I was able to bring up our board, the Linux runs correctly from the onboard eMMC,
BUT,

the LS1046's RESET_REQ_B constantly pulled down. During the reset sequence it goes high then goeas back low
Despite of this everything seems to be OK.

But I don't understand this phenomenon.

Has anybody faced this before?

thanks in advance,

Gabor

0 件の賞賛
返信
2 返答(返信)

2,433件の閲覧回数
flashingsky
Contributor II

I meet the same problem.I'm very puzzled now.

If I used the RESET_REQ_B of LS1046A to trig a power on reset. LS1046A can not bring up.

0 件の賞賛
返信

2,650件の閲覧回数
ufedor
NXP Employee
NXP Employee

Described behaviour means that there is an issue with RCW.

The first point to check is SerDes reference clocks - they should have correct frequencies and should be provided for all PLLs which are not explicitly powered down in the RCW.

In case of further question please provide the processor connection schematics as searchable PDF for inspection along with U-Boot log.

0 件の賞賛
返信