LS1043argw RGMII

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1043argw RGMII

7,150 次查看
klh
Contributor I

Hi,

I have successfully built a custom board based on LS1043argw rev B. I'm using 2016.09+fslgit-r0 uboot files.

For the custom board, the here's the changes:-

1) not using sgmii in the architecture (hence no 4 port ethernet phy in the design), using 2 X RGMII instead using AR8035 atheros phy.

 - Change rcw on bit 416 to 421 to 000000 (RGMII and RGMII2)

- Change rcw serdes protocol to 1555 (XFI, 3 x PCIE & RGMII)  (hence, technically i don't have TSEC1, TSEC2, TSEC5, TSEC6 which belongs previously to RGW reference design having Vitesse phy), i still have 10G fibre optic configuration same as RGW reference design.

- On the changes on adding PCIE3 (since I choose serdes protocol 1555), i won't discuss here, coz want to discuss only the RGMII

- On schematic, 1 x atheros AR8035 (ethernet phy) is connected to EC1 = RGMII 1 having EMI1_MDC and EMI1_MDIO connected, having physical address 1

- another atheros AR8035 (ethernet phy) is connected to EC2 = RGMII 2 having EMI2_MDC and EMI2_MDIO connected having physcial address 2

- In the make menuconfig, i have enabled ethernet portion with the driver AR8035 enabled. uboot can recognise this driver as shown in uboot log below. 

- In the ls1043argw.c file, i have added the line

fm_info_set_phy_address(FM1_DTSEC3, RGMII_PHY1_ADDR);

fm_info_set_phy_address(FM1_DTSEC4, RGMII_PHY2_ADDR);

- In the ls1043argw.h, i have added the line

#define RGMII_PHY1_ADDR            0x1

#define RGMII_PHY2_ADDR            0x2

- In the uboot log below, you can see that when I type mdio list, i can see only DTSEC3 recognised in uboot as AR8035 (which I can ping and flash software to nand without issue), but somehow I can't get RGMII2 (DTSEC4 enabled).  The error says could not get PHY for FSL_MDIO0: addr 2

=>mdio list

FSL_MDIO0:
1 - AR8035 <--> FM1@DTSEC3

Here's a snapshot of the uboot

U-Boot SPL 2016.092.0+ga06b209 (Feb 15 2019 - 16:37:26)
Initializing DDR....
Applying DDR4 workaround ......
Trying to boot from NAND


U-Boot 2016.092.0+ga06b209 (Feb 15 2019 - 16:37:26 +0800)

SoC:  LS1043AE Rev1.1 (0x87920011)
Clock Configuration:
       CPU0(A53):1600 MHz  CPU1(A53):1600 MHz  CPU2(A53):1600 MHz  
       CPU3(A53):1600 MHz  
       Bus:      400  MHz  DDR:      1600 MT/s  FMAN:     500  MHz
Reset Configuration Word (RCW):
       00000000: 08100010 0a000000 00000000 00000000
       00000010: 15550002 80004002 e0106000 c1002000
       00000020: 00000000 00000000 00000000 01030940
       00000030: 00000000 00003004 00000096 00000001
Model: LS1043A RGW Board
Board: LS1043ARGW, boot from NAND
SERDES Reference Clocks:
SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ
I2C:   ready
DRAM:  Detected UDIMM Fixed DDR on board
2 GiB (DDR4, 32-bit, CL=11, ECC off)
Retimer:
       Revision 0x03, ID 0x01
SEC0: RNG instantiated
PSCI: PSCI does not exist.
Waking secondary cores to start from ffd0d000
All (4) cores are up.
Using SERDES1 Protocol: 5461 (0x1555)
NAND:  512 MiB
MMC:   FSL_SDHC: 0
In:    serial
Out:   serial
Err:   serial
Assign to qe-tdm clk, rcwpmuxcr0=4311
Not a microcode
Net:   Fman1: Uploading microcode version 108.4.23
Could not get PHY for FSL_MDIO0: addr 2
Failed to connect
Could not get PHY for FM_TGEC_MDIO: addr 1
Failed to connect
PCIe0: pcie@3400000 Root Complex: no link
PCIe1: pcie@3500000 Root Complex: no link
PCIe2: pcie@3600000 Root Complex: no link
FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@TGEC1

Hit any key to stop autoboot:  0
=> printenv
baudrate=115200
bootargs=console=ttyS0,115200 root=/dev/ram0 earlycon=uart8250,mmio,0x21c0500
bootcmd=nand read $kernel_load $kernel_addr $kernel_size;bootm $kernel_load
bootdelay=10
console=ttyAMA0,38400n8
eth1addr=00:04:9F:04:65:11
eth2addr=00:04:9F:04:65:22
eth3addr=00:04:9F:04:65:33
eth4addr=00:04:9F:04:65:44
eth5addr=00:04:9F:04:65:55
eth6addr=00:04:9F:04:65:66
ethact=FM1@DTSEC3
ethaddr=00:04:9F:04:65:00
ethprime=FM1@DTSEC3
fdt_high=0xffffffffffffffff
fdtcontroladdr=ffc08600
fileaddr=a0000000
filesize=1fff5d3
fman_ucode=ffc29530
hwconfig=fsl_ddr:bank_intlv=auto
initrd_high=0xffffffffffffffff
ipaddr=192.168.0.3
kernel_addr=0x160000
kernel_load=0xa0000000
kernel_size=1fff5d3
kernel_start=0x61100000
loadaddr=0x80100000
mtdparts=mtdparts=60000000.nor:1m(nor_bank0_rcw),1m(nor_bank0_uboot),1m(nor_ban)
ramdisk_addr=0x800000
ramdisk_size=0x2000000
serverip=192.168.0.60
stderr=serial
stdin=serial
stdout=serial

Environment size: 1267/8188 bytes

=> mdio list
FSL_MDIO0:
1 - AR8035 <--> FM1@DTSEC3
FM_TGEC_MDIO:
=> mii info
PHY 0x01: OUI = 0x1374, Model = 0x07, Rev = 0x02, 1000baseX, HDX
=>

Kindly help, what other modifications in the file structure i need to do to enable RGMII2 (DTSEC4)? Many thanks.

标签 (1)
标记 (2)
0 项奖励
回复
10 回复数

6,619 次查看
klh
Contributor I

Sorry correction on typo should be eth.c file:-

- In the eth.c file in ls1043argw folder, i have added the line

fm_info_set_phy_address(FM1_DTSEC3, RGMII_PHY1_ADDR);

fm_info_set_phy_address(FM1_DTSEC4, RGMII_PHY2_ADDR);

0 项奖励
回复

6,619 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello kl h,

LS1043ARDB integrates two RGMII ports setting up as FM1_DTSEC3 and FM1_DTSEC4, you could do your porting based on board/freescale/ls1043ardb/eth.c.

I cannot find u-boot source code supporting ls1043argw, would you please attach your modified eth.c and ls1043argw.h? I will do some verification for you on my side.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

6,619 次查看
klh
Contributor I

Hi YiPing,

here's the attachment...

we have modified in eth.c and ls1043argw.h

the other files are for your reference, in case you need them... the 2016 uboot is a very old structure...

0 项奖励
回复

6,619 次查看
klh
Contributor I

hi, if you need me to attach the screenshot of schematics on RGMII connections, let me know. But the RGMII 1 and RGMII 2 connections are exact same IC. 

0 项奖励
回复

6,619 次查看
klh
Contributor I

one more item, on the MDC and MDIO pins on the cpu, i have pull high of 1.5kohm and 4.7kohm. Maybe it's too high resistor value? Maybe I should reduce it to 200ohm and 330ohm... ?

0 项奖励
回复

6,619 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello kl h,

Please refer to the following section in Ethernet Management Interface (EMI1/2) pin termination checklist.

EMIx_MDC could be left unconnected since it is an output.

  pastedImage_2.png

     pastedImage_3.png

I didn't find obvious problem in your modified u-boot source code. Please check the hardware design.

Thanks,

Yiping

0 项奖励
回复

6,619 次查看
klh
Contributor I

Hi Yi Ping,

Thanks for the lookup on the codes. I follow your advise and check on the hardware connections again. Apparently, during P1023, I use common mdc mdio from cpu to both the phy Ethernet @ address 1 & 2.

Here I further do the modification and connect both phy’s MDC and MDIO to EMI1_MDC and EMI1_MDIO. Now I don’t get the error anymore.

When I type mdio list, I get

FSL_MDIO0:

1 – AR8035 < - - > FM1@DTSEC3

2 – AR8035 < - - > FM1@DTSEC4

FM_TGEC_MDIO:

1 – Generic 10G PHY < - - > FM1@TGEC1

Hence, I think the code FSL_MDIO0 maybe referring to EMI1_MDC and EMI1_MDIO and not EMI2…

Regards

0 项奖励
回复

6,619 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello kl h,

Please also refer to LS1043ARDB hardware design as the following, RTL8211FS is RGMII PHY, AQR105-B1 is XFI PHY.

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

6,619 次查看
klh
Contributor I

Hi Yi Ping,

Thanks for the detailed description. It’s very clear for my modification of the design. We can now close the thread.

Actually I have another question on the I2C portion, but should continue with this or raise a new Thread in the community?

regards

0 项奖励
回复

6,619 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello kl h,

Please create a new thread in community to address you other issue to make it convenient for other customers to searching from.

Thanks,

Yiping

0 项奖励
回复