the problem of FRDM-LS1012A-PA SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the problem of FRDM-LS1012A-PA SDK

724件の閲覧回数
13540372905
Contributor I

We have bought a FRDM-LS1012A-PA board. The SDK downloaded from the official website does not support this board. Could you help us find an SDK that supports this board?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

586件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers SDK 2.0-1703 for the FRDM-LS1012A board. See the Section 4.4.6 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

586件の閲覧回数
13540372905
Contributor I

According to the document you provided, we cannot find the corresponding SDK installation package (www.nxp.com/sdk) from the download link in the third chapter of the document.

0 件の賞賛
返信

586件の閲覧回数
13540372905
Contributor I

Can you help us find the corresponding SDK v2.0-1703 installation package?

0 件の賞賛
返信