LS1043A DDR3L Address Routing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1043A DDR3L Address Routing

跳至解决方案
2,998 次查看
serkanOz
Contributor II

Hi,

We are currently designing LS1043A board with DDR3L 32+4bit interface. I have a question at that point about address matching for fly by topology. AN3940 states as follows;
"• Tune signals to +/-10 mils of the clock at each device"

What does it mean? There are two options about it.

------------------------------------------------------------------------------------------------------------------------
Board Design Address Routing;

LS1043A ----- L1 ----- |DDR3L1| ----- L2 ----- |DDR3L2| ----- L3 ----- |DDR3L3| ---- Termination

------------------------------------------------------------------------------------------------------------------------
1. Option

L1 = +/-10mil match between address-clock
L2 = +/-10mil match between address-clock
L3 = +/-10mil match between address-clock

DDR3L1 will have 10mils tolerance in worst case.
DDR3L2 will have 20mils tolerance in worst case.
DDR3L3 will have 30mils tolerance in worst case.

------------------------------------------------------------------------------------------------------------------------

2. Option
L1             = +/-10mil match between address-clock
L1+L2       = +/-10mil match between address-clock
L1+L2+L3 = +/-10mil match between address-clock

DDR3L1 will have 10mils tolerance in worst case.
DDR3L2 will have 10mils tolerance in worst case.
DDR3L3 will have 10mils tolerance in worst case.

------------------------------------------------------------------------------------------------------------------------

Which options is mentioned by AN3940? If the second option is mentioned, it is a bit strict for maximum 1600Mbit/s (for LS1043A) interface.

Have a nice day

 

标记 (3)
0 项奖励
回复
1 解答
2,979 次查看
Bulat
NXP Employee
NXP Employee

You are right, the app note says "Tune signals to +/-10 mils of the clock at each device". This statement corresponds to option 2 in your description, regardless of device position in the fly-by chain, all address/command/control signals at the device should be +/-10 mils of the clock. This is specified for 2133MT/s speed, can be slightly relaxed for 1600MT/s, but we can not provide numeric values for this relaxing.

 

Regards,

Bulat

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,980 次查看
Bulat
NXP Employee
NXP Employee

You are right, the app note says "Tune signals to +/-10 mils of the clock at each device". This statement corresponds to option 2 in your description, regardless of device position in the fly-by chain, all address/command/control signals at the device should be +/-10 mils of the clock. This is specified for 2133MT/s speed, can be slightly relaxed for 1600MT/s, but we can not provide numeric values for this relaxing.

 

Regards,

Bulat

 

 

0 项奖励
回复
2,969 次查看
serkanOz
Contributor II

Thanks for your explanation.

0 项奖励
回复