LS1043A DDR3L Address Routing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A DDR3L Address Routing

Jump to solution
2,941 Views
serkanOz
Contributor II

Hi,

We are currently designing LS1043A board with DDR3L 32+4bit interface. I have a question at that point about address matching for fly by topology. AN3940 states as follows;
"• Tune signals to +/-10 mils of the clock at each device"

What does it mean? There are two options about it.

------------------------------------------------------------------------------------------------------------------------
Board Design Address Routing;

LS1043A ----- L1 ----- |DDR3L1| ----- L2 ----- |DDR3L2| ----- L3 ----- |DDR3L3| ---- Termination

------------------------------------------------------------------------------------------------------------------------
1. Option

L1 = +/-10mil match between address-clock
L2 = +/-10mil match between address-clock
L3 = +/-10mil match between address-clock

DDR3L1 will have 10mils tolerance in worst case.
DDR3L2 will have 20mils tolerance in worst case.
DDR3L3 will have 30mils tolerance in worst case.

------------------------------------------------------------------------------------------------------------------------

2. Option
L1             = +/-10mil match between address-clock
L1+L2       = +/-10mil match between address-clock
L1+L2+L3 = +/-10mil match between address-clock

DDR3L1 will have 10mils tolerance in worst case.
DDR3L2 will have 10mils tolerance in worst case.
DDR3L3 will have 10mils tolerance in worst case.

------------------------------------------------------------------------------------------------------------------------

Which options is mentioned by AN3940? If the second option is mentioned, it is a bit strict for maximum 1600Mbit/s (for LS1043A) interface.

Have a nice day

 

Tags (3)
0 Kudos
Reply
1 Solution
2,922 Views
Bulat
NXP Employee
NXP Employee

You are right, the app note says "Tune signals to +/-10 mils of the clock at each device". This statement corresponds to option 2 in your description, regardless of device position in the fly-by chain, all address/command/control signals at the device should be +/-10 mils of the clock. This is specified for 2133MT/s speed, can be slightly relaxed for 1600MT/s, but we can not provide numeric values for this relaxing.

 

Regards,

Bulat

 

 

View solution in original post

0 Kudos
Reply
2 Replies
2,923 Views
Bulat
NXP Employee
NXP Employee

You are right, the app note says "Tune signals to +/-10 mils of the clock at each device". This statement corresponds to option 2 in your description, regardless of device position in the fly-by chain, all address/command/control signals at the device should be +/-10 mils of the clock. This is specified for 2133MT/s speed, can be slightly relaxed for 1600MT/s, but we can not provide numeric values for this relaxing.

 

Regards,

Bulat

 

 

0 Kudos
Reply
2,912 Views
serkanOz
Contributor II

Thanks for your explanation.

0 Kudos
Reply