LS1028A RDB interposer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A RDB interposer

Jump to solution
1,454 Views
mkraj
Contributor III

Dear Team

We are doing a new board design with LS1028A. We want to  remove the complete interposer interface from the existing reference board. 

We want to delete complete interposer CFG_LS1043INT_RCW_SRC1,2,4,5,6,7 signals and corresponding circuit.

Is it ok?

We want to use in Only LS1028A mode only.

Thanks in advance.

With Regards

 

 

0 Kudos
Reply
1 Solution
1,386 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, you can use only the LS1028A mode by removing the interposer part. You can also remove the CFG_LS1043INT_RCW_SRC1, 2, 4, 5, 6, 7, and CFG_LS1043INT_DRAM_TYPE signals from the CPLD.

View solution in original post

1 Reply
1,387 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, you can use only the LS1028A mode by removing the interposer part. You can also remove the CFG_LS1043INT_RCW_SRC1, 2, 4, 5, 6, 7, and CFG_LS1043INT_DRAM_TYPE signals from the CPLD.