LS1028A RDB interposer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1028A RDB interposer

跳至解决方案
1,502 次查看
mkraj
Contributor III

Dear Team

We are doing a new board design with LS1028A. We want to  remove the complete interposer interface from the existing reference board. 

We want to delete complete interposer CFG_LS1043INT_RCW_SRC1,2,4,5,6,7 signals and corresponding circuit.

Is it ok?

We want to use in Only LS1028A mode only.

Thanks in advance.

With Regards

 

 

0 项奖励
回复
1 解答
1,434 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Yes, you can use only the LS1028A mode by removing the interposer part. You can also remove the CFG_LS1043INT_RCW_SRC1, 2, 4, 5, 6, 7, and CFG_LS1043INT_DRAM_TYPE signals from the CPLD.

在原帖中查看解决方案

1 回复
1,435 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Yes, you can use only the LS1028A mode by removing the interposer part. You can also remove the CFG_LS1043INT_RCW_SRC1, 2, 4, 5, 6, 7, and CFG_LS1043INT_DRAM_TYPE signals from the CPLD.