LS1027A with DDR3L

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1027A with DDR3L

跳至解决方案
2,014 次查看
igor_franco
Contributor IV

Hello,

We are developing a custom board based on the LS1027A processor. We used the LS1028ARDB as an evaluation board to understand the functionality of the LS family. The kit uses four DDR4 of 1GB and another one as ECC. In our custom board, we want to use DDR3L instead of DDR4 (with ECC). According to the "Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces" (AN5097), the DQ swapping must consider the nibble:

igor_franco_0-1608633263975.png

However, when we read the "Hardware and Layout Design Considerations for DDR3 SDRAM Memory Interfaces" (AN3940, identified in chapter 3.1 of "QorIQ LS1028A Design Checklist", AN12028), it says that the swapping can be performed in a byte:

igor_franco_1-1608634005148.png

My question is: how can I configure the DQ mapping register x (DDR_DQ_MAPx) to allows the swap inside a byte once it considers only nibbles? Is this register ignored with DDR3L?

 

Thank you in advance,

Igor

 

0 项奖励
回复
1 解答
2,004 次查看
ufedor
NXP Employee
NXP Employee

> Is this register ignored with DDR3L?

DQ mapping is applicable for DDR4 SDRAM only.

For DDR3L DQn_MAP registers can be left with default values.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,005 次查看
ufedor
NXP Employee
NXP Employee

> Is this register ignored with DDR3L?

DQ mapping is applicable for DDR4 SDRAM only.

For DDR3L DQn_MAP registers can be left with default values.

0 项奖励
回复
1,999 次查看
igor_franco
Contributor IV

Thank you for the fast answer ufedor.

I marked it as solved.

0 项奖励
回复