ls1028ardb ethernet (msi disabled) problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1028ardb ethernet (msi disabled) problem

1,332 Views
pjw
Contributor II

We are developing custom board using ls1028.

The current problem is that Ethernet does not work when a PCI module that uses Marvell's chip is connected to the board


If  enter ifconfig after boot, eno0 and eno2 will not be checked.

After analyzing the log, it seems to be a problem to disable the msi side at the pci driver.

그림1.jpg

 


My question is, is there a way to operate ethernet regardless of msi?

Disabling msi seems to cause a problem with the irq_vector, and I wonder if we can set the irq_vector manually.

0 Kudos
Reply
1 Reply

1,304 Views
andrei_skok
NXP Employee
NXP Employee

Our Software team has requested full kernel log and the information on LSDK release you are using.

0 Kudos
Reply