LS1021ATWR eTSEC1 not functional

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021ATWR eTSEC1 not functional

Jump to solution
7,923 Views
mauryanderson
Contributor I

Greetings,

I am building SDK v1.8 for the LS1021A TWR board, using GCC 4.8.4.  I modified the U-Boot environment to boot via TFTP.  eTSEC2 and 3 work, but  eTSEC1 cannot communicate.  It establishes link at 1Gbps, however I never see Tx packets show up at the switch.  eTSEC1 sets up as eth0 in Linux, but does not work there either.

I verified that the HW is using NOR flash 0 RCW and that RCW is SSR_PPN_20.  SW2 and SW3 are at defaults.

Is there something I must do in order to get all 3 network interfaces functional?  What further information can I provide?

Thank you,

Maury Anderson

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
7,134 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Maury Anderson,

According to your u-boot log, it seems that you use RCW RSR_PPS_70/rcw_1000.bin, the setting of this RCW is 1 SGMII, 1 RGMII, 1SATA, 2PCIE, CAN, SAI, please refer to the the following SerDes options, that's why eTSEC1 cannot work. Please use RCW SSR_PPN_20/rcw_1000.bin in the pre-built image ISO, and please make sure that you flash the RCW on the correct bank.

pastedImage_0.png


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

8 Replies
7,134 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Maury Anderson,

Do you use LS1021ATWR CPU Rev1.0 or Rev2.0 board?

Would you please provide u-boot and Linux Kernel boot log?

Please setup eth0 and provide the result of "ethtool eth0".


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
7,134 Views
mauryanderson
Contributor I

Greetings Yiping,

Thank you for your response.  Here is my attempt to satisfy the request for information.  I have doubts, based on ethtool information, that we are using eTSEC1 in a valid way.

Thanks for your help,

Maury

############################################################

Revision Data

############################################################

Silkscreen on circuit card is: (c) 2014 LS-1021A

There are 3 labels on circuit card containing revision details:

700-28040 REV C

SCH-28040 REV D1

CPLD v2.3 LS1021A SDK v1.3

############################################################

Boot Output

############################################################

U-Boot 2015.01-RCLinux-NewShinyDevKit (Sep 09 2015 - 13:23:58)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 70000000 00407900 e0025a00 21046000

       00000020: 00000000 00000000 00000000 00038000

       00000030: 00080000 48007340 00000000 00000000

Board: LS1021ATWR

CPLD:  V2.3

PCBA:  V4.0

VBank: 0

I2C:   ready

DRAM:  1 GiB

Using SERDES1 Protocol: 112 (0x70)

Firmware 'Microcode version 0.0.0 for T1040 r1.0' for 1040 V1.0

QE: uploading microcode 'Microcode for T1040 r1.0'

Flash: 128 MiB

MMC:   FSL_SDHC: 0

EEPROM: CRC mismatch (3b162798 != ffffffff)

PCIe1: Root Complex no link, regs @ 0x3400000

PCIe2: Root Complex no link, regs @ 0x3500000

In:    serial

Out:   serial

Err:   serial

SEC0: RNG instantiated

SATA link 0 timeout.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc

scanning bus for devices...

Found 0 device(s).

SCSI:  Net:   eTSEC2 is in sgmii mode.

eTSEC1 [PRIME], eTSEC2, eTSEC3

Hit any key to stop autoboot:  0

eTSEC1 Waiting for PHY auto negotiation to complete. done

Speed: 1000, full duplex

Using eTSEC1 device

TFTP from server 10.10.0.1; our IP address is 10.10.0.100

Filename 'ls1021twr0/uImage'.

Load address: 0x80020000

Loading: T T T T T T T T T T

Retry count exceeded; starting again

Speed: 1000, full duplex

Using eTSEC2 device

TFTP from server 10.10.0.1; our IP address is 10.10.0.100

Filename 'ls1021twr0/ls1021a-twr.dtb'.

Load address: 0x80000000

Loading: ##

         1.5 MiB/s

done

Bytes transferred = 21046 (5236 hex)

Speed: 1000, full duplex

Using eTSEC2 device

TFTP from server 10.10.0.1; our IP address is 10.10.0.100

Filename 'ls1021twr0/rootfs.cpio.uboot'.

Load address: 0x81000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         ################################

         1.7 MiB/s

done

Bytes transferred = 4279911 (414e67 hex)

## Booting kernel from Legacy Image at 80020000 ...

   Image Name:   Linux-3.12.37-rt51-RCLinux-Maury

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3105160 Bytes = 3 MiB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 81000000 ...

   Image Name:

   Image Type:   ARM Linux RAMDisk Image (uncompressed)

   Data Size:    4279847 Bytes = 4.1 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 80000000

   Booting using the fdt blob at 0x80000000

   Loading Kernel Image ... OK

   Loading Ramdisk to beb0f000, end bef23e27 ... OK

   Loading Device Tree to beb06000, end beb0e235 ... OK

Starting kernel ...

i2c i2c-2: of_i2c: modalias failure on /soc/i2c@21a0000/ltc2945@67

layerscape-pcie 3400000.pcie: phy link never came up

layerscape-pcie 3500000.pcie: phy link never came up

sgtl5000 1-000a: Failed to get supply 'VDDD': -19

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

Starting logging: OK

Initializing random number generator... done.

Starting network...

udhcpc (v1.23.1) started

Sending discover...

Sending discover...

Sending discover...

Sending select for 10.10.1.74...

Lease of 10.10.1.74 obtained, lease time 86400

adding dns 10.10.0.1

Welcome to Linux

devkit login:

############################################################

Ethtool Output

############################################################

# ethtool eth0

Settings for eth0:

        Supported ports: [ MII ]

        Supported link modes:   10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

                                1000baseT/Full

        Supported pause frame use: Symmetric Receive-only

        Supports auto-negotiation: Yes

        Advertised link modes:  10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

                                1000baseT/Full

        Advertised pause frame use: No

        Advertised auto-negotiation: Yes

        Speed: 1000Mb/s

        Duplex: Full

        Port: MII

        PHYAD: 2

        Transceiver: external

        Auto-negotiation: on

        Supports Wake-on: uag

        Wake-on: d

        Current message level: 0x0000003f (63)

                               drv probe link timer ifdown ifup

        Link detected: yes

#

0 Kudos
Reply
7,135 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Maury Anderson,

According to your u-boot log, it seems that you use RCW RSR_PPS_70/rcw_1000.bin, the setting of this RCW is 1 SGMII, 1 RGMII, 1SATA, 2PCIE, CAN, SAI, please refer to the the following SerDes options, that's why eTSEC1 cannot work. Please use RCW SSR_PPN_20/rcw_1000.bin in the pre-built image ISO, and please make sure that you flash the RCW on the correct bank.

pastedImage_0.png


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

6,713 Views
Xi-nanWang
Contributor II

Based on this tab, I wonder how can I use eTSEC0 as SGMII , eTSEC1 and eTSEC2 as RGMII, it seems like SGMII1 and SGMII2 must be configured at the same time

Tags (1)
0 Kudos
Reply
7,134 Views
romitchatterjee
Contributor V

I am facing same issue i.e eTSEC1 is not working while eTSEC2 and eTSEC3 are working. I have posted this in below thread.

https://community.nxp.com/thread/439364 

Any help is highly appreciated.

0 Kudos
Reply
7,134 Views
dusanferbas
Contributor III

Hi Romit, I posted comment here, where I described that I think the MUX is improperly switched. Noone said I am wrong, noone posted a CPLD source matching the label on our Tower board.

0 Kudos
Reply
7,134 Views
romitchatterjee
Contributor V

Hi Dusan,

Thanks for your reply. I think MUX is properly switched and also according to board specification (TWR-LS1021ARM), eTSEC ports do not depend on any switch setting.

Are you still facing this issue of eTSEC1 not working while eTSEC2 and eTSEC3 are working? Have you found any solution?

0 Kudos
Reply
7,134 Views
nagireddychitta
Contributor III

Hi,

I see this is relevant thread to post my rcw_1000.rcw recompilation issue.

My custom board is bit different than the reference board LS1021TWR, so i have modified the RCW bits according to my board using CW dev studio+QCVS tool and using it.

I want to include this as part of Yocto tree and build it along with other images(linux kernel,u-boot,RFS etc).

So i had generated pbl.pbl file from CW dev studio and modified rcw_1000.rcw file under /rcw/git-r0/git/nextflash/SSR_PNS_30/ path,but the issue is only when i do the cleanstate build using bitbake it builds this file else it will not recompile this file.

If someone is aware of how to recompile without doing cleanstate with bitbake(as it takes nearly 1 hour to recompile the tree),kindly help me out.

Best Regards,

Nagi

0 Kudos
Reply