LS1021A: PCIe: using multiple MSIs for one EP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A: PCIe: using multiple MSIs for one EP

1,490件の閲覧回数
alexanderstein
Contributor II

I need to create a PCIe extension card which must support multiple MSIs, not MSI-X which is not possible on the card. Reading the LS1021A Reference Manual (Rev. 0, 11/2015) 10.2.47 SCFG_PEXMSIIR is the register which must be programmed as the Message Address Register to PCIe EP. The current driver pcie-designware + pci-layerscape does this.

So when a MSI occures the MSI Message Data contains the MSI number, e.g. 0h, 1h, 2h and so on, which is written to SCFG_PEXMSIIR in little-endian. Now reading the register definition IBS, containing the lowest byte of MSI Message Data, ignores the lowest 3 bits at all. MSI requires that MSi numbers are consequtive for one EP. How is this supposed to work if the lowest bits are ignored at all?

ラベル(1)
タグ(1)
0 返答(返信)