SDK 2.0 for ls1043ardb failed to recognize NOR flash on kernel start up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK 2.0 for ls1043ardb failed to recognize NOR flash on kernel start up

1,118件の閲覧回数
hoanguyen
Contributor II

I rebuilt sdk 2.0 for the ls1043ardb without any change. I noticed that the NOR flash was not recognized as follows:

 

[    0.232235] scsi host0: ahci-qoriq

[    0.235739] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 30

[    0.245089] of-flash 60000000.nor: do_map_probe() failed for type cfi_probe

[    0.252104] of-flash 60000000.nor: do_map_probe() failed

 

Executing the following command got:

 

root@ls1043ardb:~# cat /proc/mtd

dev:    size   erasesize  name

mtd0: 20000000 00020000 "7e800000.flash"

mtd1: 01000000 00010000 "spi0.0"

 

the entire startup log is attached!

 

Do anyone know how to fix this problem?

 

thanks,

Hoa

Original Attachment has been moved to: NOR_failed.txt.zip

ラベル(1)
0 件の賞賛
返信
1 返信

935件の閲覧回数
Pavel
NXP Employee
NXP Employee

Usually u-boot provides NOR Flash configuration. Linux uses configuration from u-boot.

Is there problem for using NOR Flash under u-boot on your board.

U-boot configuration file is located in the u-boot source folder: /include/configs. This folder contains the .h files for the different boards.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信