LS1021A: PCIe: using multiple MSIs for one EP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021A: PCIe: using multiple MSIs for one EP

1,123 次查看
alexanderstein
Contributor II

I need to create a PCIe extension card which must support multiple MSIs, not MSI-X which is not possible on the card. Reading the LS1021A Reference Manual (Rev. 0, 11/2015) 10.2.47 SCFG_PEXMSIIR is the register which must be programmed as the Message Address Register to PCIe EP. The current driver pcie-designware + pci-layerscape does this.

So when a MSI occures the MSI Message Data contains the MSI number, e.g. 0h, 1h, 2h and so on, which is written to SCFG_PEXMSIIR in little-endian. Now reading the register definition IBS, containing the lowest byte of MSI Message Data, ignores the lowest 3 bits at all. MSI requires that MSi numbers are consequtive for one EP. How is this supposed to work if the lowest bits are ignored at all?

标签 (1)
标记 (1)
0 回复数