LS1012A eSDHC Pull-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A eSDHC Pull-up

Jump to solution
1,917 Views
jaredl
Contributor I

Does the "Pull up" column in Table 18-4 of the reference manual (LS1012ARM) indicate that the LS1012A has internal pull-ups on these signals or does it indicate that external pull-ups are required?

jaredl_0-1613596597912.pngjaredl_0-1613596597912.png

 

0 Kudos
Reply
1 Solution
1,906 Views
andrei_skok
NXP Employee
NXP Employee
According to the LS1012A Datasheet, Table 1. Pinout list by bus, notes 28,29
 
and 
 
LS1012A Design checklist, 5.4.1 eSDHC pin termination recommendations
 
SDHCx_CMD and SDHCx_DAT[0:3] pins should be pulled high through a 10-20 kΩ resistor to EVDD.

View solution in original post

0 Kudos
Reply
1 Reply
1,907 Views
andrei_skok
NXP Employee
NXP Employee
According to the LS1012A Datasheet, Table 1. Pinout list by bus, notes 28,29
 
and 
 
LS1012A Design checklist, 5.4.1 eSDHC pin termination recommendations
 
SDHCx_CMD and SDHCx_DAT[0:3] pins should be pulled high through a 10-20 kΩ resistor to EVDD.
0 Kudos
Reply