LS1012A eSDHC Pull-up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A eSDHC Pull-up

ソリューションへジャンプ
1,960件の閲覧回数
jaredl
Contributor I

Does the "Pull up" column in Table 18-4 of the reference manual (LS1012ARM) indicate that the LS1012A has internal pull-ups on these signals or does it indicate that external pull-ups are required?

jaredl_0-1613596597912.png

 

0 件の賞賛
返信
1 解決策
1,949件の閲覧回数
andrei_skok
NXP Employee
NXP Employee
According to the LS1012A Datasheet, Table 1. Pinout list by bus, notes 28,29
 
and 
 
LS1012A Design checklist, 5.4.1 eSDHC pin termination recommendations
 
SDHCx_CMD and SDHCx_DAT[0:3] pins should be pulled high through a 10-20 kΩ resistor to EVDD.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,950件の閲覧回数
andrei_skok
NXP Employee
NXP Employee
According to the LS1012A Datasheet, Table 1. Pinout list by bus, notes 28,29
 
and 
 
LS1012A Design checklist, 5.4.1 eSDHC pin termination recommendations
 
SDHCx_CMD and SDHCx_DAT[0:3] pins should be pulled high through a 10-20 kΩ resistor to EVDD.
0 件の賞賛
返信