LS1012A-RDB eMMC flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A-RDB eMMC flash

ソリューションへジャンプ
9,497件の閲覧回数
bgreen
Contributor II

I'd like to set up the eMMC flash on the LS1012A-RDB. I've set the DIP switch to select the eMMC flash on SDHC2 but after booting up I get the error:

mmc1: Controller never released inhibit bit(s).

This message scrolls forever. The SD card on SDHC1 works fine. This is using the LS1012A SDK Rev 0.4

ラベル(1)
1 解決策
8,649件の閲覧回数
bgreen
Contributor II

I have discovered the source of my problem. When originally setting up QSPI bank 2, I copied over the RCW and u-boot from QSPI bank 1. These images are from the BHR ASK (I assume). I then loaded u-boot, kernel, and ppa images from the SDK, but not the RCW. Not loading the correct RCW was the source of my problem. After loading the SDK RCW (PBL_0x35_0x08_800_250_1000_default.bin) the eMMC flash came up correctly.

元の投稿で解決策を見る

11 返答(返信)
8,650件の閲覧回数
bgreen
Contributor II

I have discovered the source of my problem. When originally setting up QSPI bank 2, I copied over the RCW and u-boot from QSPI bank 1. These images are from the BHR ASK (I assume). I then loaded u-boot, kernel, and ppa images from the SDK, but not the RCW. Not loading the correct RCW was the source of my problem. After loading the SDK RCW (PBL_0x35_0x08_800_250_1000_default.bin) the eMMC flash came up correctly.

8,649件の閲覧回数
ufedor
NXP Employee
NXP Employee

> I've set the DIP switch to select the eMMC flash

What exactly you have done?

0 件の賞賛
返信
8,649件の閲覧回数
bgreen
Contributor II

On the LS1012A-RDB there is an LS1012A with 2 SDHC interfaces. SDHC2 is connected to a mux which can select between several different on-board devices using a DIP switch. I have set the switch to:

MUX_SDHC2_S1: 1
MUX_SDHC2_S0: 0

According to the manual this should connect SDHC2 to the onboard eMMC flash. Using the images provided in the SDK I get the error mentioned above.

0 件の賞賛
返信
8,649件の閲覧回数
ufedor
NXP Employee
NXP Employee

What is the component schematics name printed on the PCB, what are the switches positions?

0 件の賞賛
返信
8,649件の閲覧回数
bgreen
Contributor II

CPU: LS1012A+ SKT LGA 211

3x MUX: 74CBTLV3253DS

eMMC: MTFC4GACAAAM-1M WT

DIP Switches (From left to right on the board)

DIP SW1: 0b11100100

DIP SW2: 0b01000010

In Particular the ones dealing with the eMMC flash are:

MUX_SDHC2_S1: 1
MUX_SDHC2_S0: 0

0 件の賞賛
返信
8,649件の閲覧回数
ufedor
NXP Employee
NXP Employee

> MUX_SDHC2_S1: 1
> MUX_SDHC2_S0: 0

To which DIP SW these settings corresponds?

Please provide a clear photo of the switches.

0 件の賞賛
返信
8,650件の閲覧回数
bgreen
Contributor II

DIPSW.png

These are the switches on the board, except the settings are (from left to right):

11100100 01000010

Where 1 is up and 0 is down.

0 件の賞賛
返信
8,650件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which configuration is on the photo?

Which switches you have altered?

0 件の賞賛
返信
8,650件の閲覧回数
bgreen
Contributor II

Shown in the Image:

10100110 00000000

Default that ships with the board:

11100100 00000000

Current board settings:

11100100 01000010

The first two bits of the second switch connect SDHC2 to the eMMC flash, the last two bits of the second switch select booting from the second bank of QSPI flash.

From the default setup that ships with the board I have changed the bit labeled MUX_SDHC2_S1 from 0 to 1, and the bit labeled MUX_QSPI_S0 from 0 to 1.

From the switches in the image the differences are:

SW_ENG_USE: 0 -> 1

UART_MUX_EN_B: 1 -> 0

MUX_SDHC2_S1: 0 -> 1

MUX_QSPI_S0: 0 -> 1

0 件の賞賛
返信
8,651件の閲覧回数
ufedor
NXP Employee
NXP Employee

> From the default setup that ships with the board I have changed the bit

> labeled MUX_SDHC2_S1 from 0 to 1, and the bit labeled MUX_QSPI_S0 from 0 to 1.

Please clarify this statement because default setup for these bits is 00.

0 件の賞賛
返信
8,651件の閲覧回数
bgreen
Contributor II

The defaults are 0 and 0. I changed them both to 1. Changing MUX_SDHC2_S1 should let me use the eMMC flash. Changing MUX_QSPI_S0 lets me boot from the second QSPI flash bank.

0 件の賞賛
返信