LS1012A RDB Default DIP Settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A RDB Default DIP Settings

2,004 Views
ScottKerstein
Contributor III

Hello,

When i power up the LS1012A RDB, the mbed mass storage device folder appears, but in the Device Manager under the COM port tree, no COM port is assigned even though I'm connected to the USB console port.  This prevents me from using a terminal program to view the booting process.

What are the default DIP switch settings for SW1 and SW2 as shipped from the factory?"

My customer fears he bricked the SPI Flash and need to determine if he really did by looking at the booting sequence.

Thanks, in advance

Scott

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,793 Views
addiyi
NXP Employee
NXP Employee

Please verify that mbed USB driver is installed. Use http://mbed.org/handbook/Windows-serial-configuration for references.

Adrian

0 Kudos
Reply

1,793 Views
sinanakman
Senior Contributor III

Hi Scott

Complete default switch configuration is listed in QorIQ LS1012A

Reference Design Board Getting Started Guide in Chapter 12 (you

need to register to download the document).

Can you verify with your customer that they are powering the board

via 12V external power supply and not only via USB.

Hope this helps

Regards

Sinan Akman

0 Kudos
Reply