LS1012A DRAM recommendation.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A DRAM recommendation.

ソリューションへジャンプ
2,106件の閲覧回数
Woon
Contributor III

I will make a custom board based on LS1012A FRWY.

but when I checked the BOM, the DRAM was discontinued.

do you have any recommended DRAM list for that?

or could you recommend which DRAM is suitable for LS1012A

 

Best regards

 

0 件の賞賛
返信
1 解決策
2,094件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Woon,

There is no such recommended DRAM list from the NXP. You can select a DRAM based on the specification of the MMDC of LS1012A or you can simply ask the DRAM vendor for the replacement of the discontinued one.

Regards,
Mrudang

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,095件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Woon,

There is no such recommended DRAM list from the NXP. You can select a DRAM based on the specification of the MMDC of LS1012A or you can simply ask the DRAM vendor for the replacement of the discontinued one.

Regards,
Mrudang

0 件の賞賛
返信