LS1012A DRAM recommendation.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A DRAM recommendation.

Jump to solution
2,108 Views
Woon
Contributor III

I will make a custom board based on LS1012A FRWY.

but when I checked the BOM, the DRAM was discontinued.

do you have any recommended DRAM list for that?

or could you recommend which DRAM is suitable for LS1012A

 

Best regards

 

0 Kudos
Reply
1 Solution
2,096 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Woon,

There is no such recommended DRAM list from the NXP. You can select a DRAM based on the specification of the MMDC of LS1012A or you can simply ask the DRAM vendor for the replacement of the discontinued one.

Regards,
Mrudang

View solution in original post

0 Kudos
Reply
1 Reply
2,097 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Woon,

There is no such recommended DRAM list from the NXP. You can select a DRAM based on the specification of the MMDC of LS1012A or you can simply ask the DRAM vendor for the replacement of the discontinued one.

Regards,
Mrudang

0 Kudos
Reply