Is it possible to change the FPGA base address on LS1046A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to change the FPGA base address on LS1046A?

Jump to solution
381 Views
2sanghaesea
Contributor II

Hello,

I’m working with a custom board based on the LS1046A.
Previously, the FPGA on our board was mapped to the memory region starting at 0x7FB0_XXXX.

Now, I would like to modify the configuration so that multiple FPGAs can each use a different memory region in the 0x7FBX_XXXX range (e.g., 0x7FB1_XXXX, 0x7FB2_XXXX, etc.).

Is it possible to change the FPGA base address to different regions within this range? If so, where should this be configured — in the device tree, RCW, or elsewhere?

Thank you for your support.

0 Kudos
Reply
1 Solution
336 Views
June_Lu
NXP TechSupport
NXP TechSupport

I could not get your question of " is it still possible to change the base address for each FPGA?".

But you could change the base address on LS1046A, please kindly refer the

LS1043A Interfacing with CPLD in LS1043ARDB Application Note 

AN12098: This document explains how IFC interface is used to connect the LS1043A processor and CPLD used on the LS1043A reference design board (RDB).

That would be similar to LS1046A.

Regards,

View solution in original post

0 Kudos
Reply
2 Replies
337 Views
June_Lu
NXP TechSupport
NXP TechSupport

I could not get your question of " is it still possible to change the base address for each FPGA?".

But you could change the base address on LS1046A, please kindly refer the

LS1043A Interfacing with CPLD in LS1043ARDB Application Note 

AN12098: This document explains how IFC interface is used to connect the LS1043A processor and CPLD used on the LS1043A reference design board (RDB).

That would be similar to LS1046A.

Regards,

0 Kudos
Reply
369 Views
2sanghaesea
Contributor II

For additional context:
Our board does not use NOR flash and boots from eMMC.
All IFC chip selects (CS0 to CS4) are connected to FPGAs.
Given this setup, is it still possible to change the base address for each FPGA?

0 Kudos
Reply