How to access SRAM using IFC in Linux?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to access SRAM using IFC in Linux?

ソリューションへジャンプ
2,505件の閲覧回数
hakjunoh
Contributor III

Hello.

We making a custom board by referring to LS1043A. Booting is the same as the reference board, and it seems to be boot from SDHC.
But after booting into Linux, we need to read/write data to SRAM.

In this case, there are two questions.

1. how to change the device tree?
In general, the device tree as follows:

&ifc {
status = "okay";
#address-cells = <2>;
#size-cells = <1>;
/* NOR, NAND Flashes and FPGA on board */
ranges = <0x0 0x0 0x0 0x60000000 0x08000000
0x1 0x0 0x0 0x7e800000 0x00010000
0x2 0x0 0x0 0x7fb00000 0x00000100>;

nor@0,0 {
compatible = "cfi-flash";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x0 0x0 0x8000000>;
big-endian;
bank-width = <2>;
device-width = <1>;
};

nand@1,0 {
compatible = "fsl,ifc-nand";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x1 0x0 0x10000>;
};

cpld: board-control@2,0 {
compatible = "fsl,ls1043ardb-cpld";
reg = <0x2 0x0 0x0000100>;
};
};

But if use SRAM instead of NAND, How to modified? Especially compatible.

Second, if the device is recognized by IFC, how should it be used?
Previously, it was recognized as MTD but SRAM needs to input/output raw data. Can I use it as it is?

Best regards.
Thanks.

タグ(2)
0 件の賞賛
返信
1 解決策
2,489件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

SRAM should be connected to IFC in GPCM mode, but we don't have GPCM driver for ARM processors. You need to develop by yourself. You can take eLBC/GPCM driver for PowerPC as reference.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,490件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

SRAM should be connected to IFC in GPCM mode, but we don't have GPCM driver for ARM processors. You need to develop by yourself. You can take eLBC/GPCM driver for PowerPC as reference.

0 件の賞賛
返信