LS1046ARDB NET-SNMP service cross-compile

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046ARDB NET-SNMP service cross-compile

9,286件の閲覧回数
Ghouse
Contributor V

I have build net-snmp in ubantu 18.04.

./configure using cross compiler fsl-qoriql arrch64-fsl-linux-gnu, i am able to run service in ubuntu 18.04 successfully, but target machine is showing

./snmpd -d -f -L

warning: no access control information configured

[config search path: /ncs/etc/snmp:/ncs/share/snmp:/ncs/lib/snmp:/root/.snmp]

Run snmpconf -g basic-setup to help you configure the snmpd.conf file for this agent.

service is started but I am not able to get the agent response in client side here are the attached screenshots. 

please help to get it sort it out.

0 件の賞賛
返信
2 返答(返信)

9,256件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please run the following command to configure and generate snmpd.conf in /ncs/share/snmp

$cd /ncs

$ perl ./bin/snmpconf -i

Please refer to the following link to configure snmpd.conf file for the agent.

https://kb.juniper.net/InfoCenter/index?page=content&id=KB25949

Then run command

./sbin/snmpd -d -f -L

0 件の賞賛
返信

9,285件の閲覧回数
Ghouse
Contributor V

leftover screenshots are here... please refer it. maximum 5 only i can share so here attached remaining.

0 件の賞賛
返信