How do I create the NOR images for LS1043ARDB on OpenIL?
I have already tried sdcard.img and it works.
I need to perform the NOR image creation through OpenIL and later perform its installation on LS1043ARDB.
Solved! Go to Solution.
Open Industrial Linux User Guide, Section 3.5.1 states:
OpenIL supports only the SD card boot mode for LS1043ARDB and the LS1046ARDB platforms.
So, there are is no ready solution. Consider using NXP LSDK:
Best Regards,
Platon
Open Industrial Linux User Guide, Section 3.5.1 states:
OpenIL supports only the SD card boot mode for LS1043ARDB and the LS1046ARDB platforms.
So, there are is no ready solution. Consider using NXP LSDK:
Best Regards,
Platon