How do I create and install the NOR images for LS1043ARDB through OpenIL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I create and install the NOR images for LS1043ARDB through OpenIL?

Jump to solution
763 Views
ts1234
Contributor III

How do I create the NOR images for LS1043ARDB on OpenIL?

I have already tried sdcard.img and it works.

I need to perform the NOR image creation through OpenIL and later perform its installation on LS1043ARDB.

0 Kudos
1 Solution
747 Views
bpe
NXP Employee
NXP Employee

Open Industrial Linux User Guide, Section 3.5.1 states:

OpenIL supports only the SD card boot mode for LS1043ARDB and the LS1046ARDB platforms.

So, there are is no ready solution. Consider using NXP LSDK:

 

https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-47B8F1F5-3A8F-45F4-A...

 

Best Regards,
Platon

View solution in original post

1 Reply
748 Views
bpe
NXP Employee
NXP Employee

Open Industrial Linux User Guide, Section 3.5.1 states:

OpenIL supports only the SD card boot mode for LS1043ARDB and the LS1046ARDB platforms.

So, there are is no ready solution. Consider using NXP LSDK:

 

https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-47B8F1F5-3A8F-45F4-A...

 

Best Regards,
Platon