Enable network manager and modem manager for ls1012a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable network manager and modem manager for ls1012a

Jump to solution
3,793 Views
kai_wu
Contributor III

Hi,

I am using lsdk2.04 now. I just downloaded the images and root file system using the command below:

       flex-installer -i download -m ls1012ardb

In the root file system rootfs_lsdk2004_ubuntu_main_arm64.tgz, I didn't find network manager and modem manager(nmcli and mmcli)

When I tried to do apt-get install network-manager,  I got these errors.

W: Failed to fetch http://us.ports.ubuntu.com/ubuntu-ports/dists/bionic/InRelease Temporary failure resolving 'apac.nics.nxp.com'
W: Failed to fetch http://us.ports.ubuntu.com/ubuntu-ports/dists/bionic-updates/InRelease Temporary failure resolving 'apac.nics.nxp.com'
W: Failed to fetch http://ports.ubuntu.com/ubuntu-ports/dists/bionic-security/InRelease Temporary failure resolving 'apac.nics.nxp.com'
W: Some index files failed to download. They have been ignored, or old ones used instead.

In 

Is there any way I can integrate nmcli and mmcli to our root file system?

Thank you!!

Labels (2)
0 Kudos
Reply
1 Solution
3,757 Views
kai_wu
Contributor III

Sorry, it's a stupid mistake.

I resolved this already.

I forgot to enable internet access. There is no internet access at all.

After enabling internet access,

I did apt-get install network-manager, nmcli and mmcli is installed successully.

NetworManager.service failed to be started. I ran apt-get remove network-manager and reinstalled it.

It works now.

View solution in original post

0 Kudos
Reply
1 Reply
3,758 Views
kai_wu
Contributor III

Sorry, it's a stupid mistake.

I resolved this already.

I forgot to enable internet access. There is no internet access at all.

After enabling internet access,

I did apt-get install network-manager, nmcli and mmcli is installed successully.

NetworManager.service failed to be started. I ran apt-get remove network-manager and reinstalled it.

It works now.

0 Kudos
Reply