Enable network manager and modem manager for ls1012a

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Enable network manager and modem manager for ls1012a

跳至解决方案
3,773 次查看
kai_wu
Contributor III

Hi,

I am using lsdk2.04 now. I just downloaded the images and root file system using the command below:

       flex-installer -i download -m ls1012ardb

In the root file system rootfs_lsdk2004_ubuntu_main_arm64.tgz, I didn't find network manager and modem manager(nmcli and mmcli)

When I tried to do apt-get install network-manager,  I got these errors.

W: Failed to fetch http://us.ports.ubuntu.com/ubuntu-ports/dists/bionic/InRelease Temporary failure resolving 'apac.nics.nxp.com'
W: Failed to fetch http://us.ports.ubuntu.com/ubuntu-ports/dists/bionic-updates/InRelease Temporary failure resolving 'apac.nics.nxp.com'
W: Failed to fetch http://ports.ubuntu.com/ubuntu-ports/dists/bionic-security/InRelease Temporary failure resolving 'apac.nics.nxp.com'
W: Some index files failed to download. They have been ignored, or old ones used instead.

In 

Is there any way I can integrate nmcli and mmcli to our root file system?

Thank you!!

标签 (2)
0 项奖励
回复
1 解答
3,737 次查看
kai_wu
Contributor III

Sorry, it's a stupid mistake.

I resolved this already.

I forgot to enable internet access. There is no internet access at all.

After enabling internet access,

I did apt-get install network-manager, nmcli and mmcli is installed successully.

NetworManager.service failed to be started. I ran apt-get remove network-manager and reinstalled it.

It works now.

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,738 次查看
kai_wu
Contributor III

Sorry, it's a stupid mistake.

I resolved this already.

I forgot to enable internet access. There is no internet access at all.

After enabling internet access,

I did apt-get install network-manager, nmcli and mmcli is installed successully.

NetworManager.service failed to be started. I ran apt-get remove network-manager and reinstalled it.

It works now.

0 项奖励
回复