We're attempting to bring up a custom board based on the NXP LS1046A SoC. We're currently struggling with DDR initialization errors in BL2 (ATF). After experimenting with the DDR controller settings, we see one of the following three outcomes:
#include <ls1046a.rcwi> /* clocking */ SYSCLK_FREQ=600             /* SYSCLK input             = 600 * 166.667 kHz =  100 MHz */ SYS_PLL_RAT=4               /* platform clock           =  4 * SYSCLK       =  400 MHz */ MEM_PLL_RAT=16              /* DDR clock                = 16 * SYSCLK       = 1600 MHz */ CGA_PLL1_RAT=12             /* PLL1 (CPU)               = 12 * SYSCLK       = 1200 MHz */ CGA_PLL2_RAT=12             /* PLL2 (FMan, eSDHC, QSPI) = 12 * SYSCLK       = 1200 MHz */ C1_PLL_SEL=0                /* CPU core clock           = PLL1 /1           = 1200 MHz */ HWA_CGA_M1_CLK_SEL=6        /* FMan clock               = PLL2 /2           =  600 MHz */ HWA_CGA_M2_CLK_SEL=1        /* eSDHC*6, QSPI*64 clocks  = PLL2 /1           = 1200 MHz */ DDR_REFCLK_SEL=1            /* use differential SYSCLK, not DDRCLK, for DDR PLL */ /* I/O bank voltages */ TVDD_VSEL=1                 /* TVDD I/O domain: 2.5 V */ DVDD_VSEL=2                 /* DVDD I/O domain: 3.3 V */ EVDD_VSEL=2                 /* EVDD I/O domain: 3.3 V */ /* SerDes 1 settings */ SRDS_PRTCL_S1=4403          /* 0x1133: 0=XFI.9, 1=XFI.10, 2=SGMII.5, 3=SGMII.6 */ SRDS_REFCLK_SEL_S1=0        /* use separate reference clocks for PLL1 and PLL2 */ SRDS_PLL_PD_S1=2            /* power down PLL1 */ SRDS_PLL_REF_CLK_SEL_S1=3   /* PLL1 @ N/A, PLL2 @ 156.25 MHz */ /* SerDes 2 settings */ SRDS_PRTCL_S2=21879         /* 0x5577: 0=PCIe.1 x1, 1=PCIe.2 x1, 2/3=PCIe.3 x2 */ SRDS_REFCLK_SEL_S2=0        /* use separate reference clocks for PLL1 and PLL2 */ SRDS_PLL_REF_CLK_SEL_S2=3   /* PLL1 @ 100 MHz, PLL2 @ 100 MHz */ SRDS_DIV_PEX_S2=0           /* PCIe can train up to 8 Gb/s */ /* memory settings */ DDR_FDBK_MULT=2             /* (reserved) DDR PLL feedback path selection and multiplication enabler */ DRAM_LAT=1                  /* 8-8-8 or higher latency DRAMs */ /* boot settings */ PBI_src=6                   /* fetch pre-boot initialization data from SD/MMC */ SB_EN=0                     /* secure boot is not enabled */ /* pin multiplexing */ IFC_GRP_A_EXT=1             /* use QSPI A signals, not FTM5, GPIO or IFC */ IFC_GRP_D_EXT=1             /* use QSPI B signals, not FTM6, GPIO or IFC */ IFC_GRP_E1_BASE=1           /* use GPIO2 signals, not FTM7, IFC or QSPI B DATA3 */ IFC_GRP_F_EXT=1             /* use QSPI A signals, not IFC */ IIC2_EXT=1                  /* use SDHC_CD_B and SDHC_WP, not IIC2/GPIO/FTM */ IRQ_OUT=1                   /* (reserved) */ IRQ_BASE=1                  /* use GPIO, not IRQ */ UART_BASE=4                 /* use UART1 SOUT/SIN/RTS/CTS and GPIO1_[16:22]*/ USB_DRVVBUS=1               /* use GPIO4[29], not USB_DRVVBUS */ USB_PWRFAULT=1              /* use GPIO4[30], not USB_PWRFAULT */ EC1=5                       /* use FTM1 */ EC2=5                       /* use FTM1 */ EM1=1                       /* use GPIO_3 */ EM2=1                       /* use GPIO_4 */ /* Pre-Boot Initialization (PBI). This PBI code mostly derives  * from the LS1046A RDB sample (rcw_1800_emmcboot.rcw). */ .pbi // SCFG_SCRATCHRW[1:2]: 64-bit boot pointer // 0x10000000 is 64 KiB on-chip RAM (OCRAM1); PBL loads BL2 here write 0x570600, 0x00000000 write 0x570604, 0x10000000 .end #include <cci_barrier_disable.rcw>  // CCI: all master interfaces terminate barriers (why?) #include <usb_phy_freq.rcw>         // take USB1, USB2 and USB3 PHYs out of reset #include <pex_gen3_link.rcw>        // PCIe errata A-010477, A-008851 (re: Gen 3) #include <a009531.rcw>              // PCIe erratum A-009531 (re: ID0 bit)  | 
DDR initialization code was generated by the latest version of QCVS running in CodeWarrior 11.5.0 on a Windows PC.
const struct ddr_cfg_regs static_1600 = {     .cs[0].bnds = 0xFF,     .cs[1].bnds = 0x0100013F,     .cs[0].config = 0x80010512,     .cs[1].config = 0x0202,     .cs[2].bnds = 0x0140017F,     .cs[3].bnds = 0x018001BF,     .cs[2].config = 0x0202,     .cs[3].config = 0x0202,     .cs[0].config_2 = 0x00,     .cs[1].config_2 = 0x00,     .cs[2].config_2 =  0x00,     .cs[3].config_2 =  0x00,     .sdram_cfg[0] = 0xC52C0000,     .sdram_cfg[1] = 0x00401030,     .timing_cfg[0] = 0xFF550018,     .timing_cfg[1] = 0xBAB40C52,     .timing_cfg[2] = 0x0048D11C,     .timing_cfg[3] = 0x01161000,     .timing_cfg[4] = 0xD501,     .timing_cfg[5] = 0x03401400,     .timing_cfg[7] = 0x23340000,     .timing_cfg[8] = 0x02116600,     .dq_map[0] = 0x32C57554,     .dq_map[1] = 0xD4BB0BD4,     .dq_map[2] = 0x2EC2F554,     .dq_map[3] = 0xD8000000,     .sdram_mode[0] = 0x01010210,     .sdram_mode[1] = 0x00,     .sdram_mode[2] = 0x00,     .sdram_mode[3] = 0x00,     .sdram_mode[4] = 0x00,     .sdram_mode[5] = 0x00,     .sdram_mode[6] = 0x00,     .sdram_mode[7] = 0x00,     .sdram_mode[8] = 0x0701,     .sdram_mode[9] = 0x04800000,     .sdram_mode[10] = 0x00,     .sdram_mode[11] = 0x00,     .sdram_mode[12] = 0x00,     .sdram_mode[13] = 0x00,     .sdram_mode[14] = 0x00,     .sdram_mode[15] = 0x00,     .md_cntl = 0x00,     .interval = 0x18600618,     .data_init = 0xDEADBEEF,     .clk_cntl = 0x02800000,     .init_addr = 0x00,     .ddr_sr_cntr = 0x0,     .init_ext_addr = 0x00,     .zq_cntl = 0x8A090705,     .wrlvl_cntl[0] = 0x86750606,     .wrlvl_cntl[1] = 0x0606060B,     .wrlvl_cntl[2] = 0x0B0C0C00,     .cdr[0] = 0x80040000,     .cdr[1] = 0x81, };  | 
INFO:    RCW BOOT SRC is SD/EMMC INFO:    RCW BOOT SRC is SD/EMMC INFO:    esdhc_emmc_init INFO:    Card detected successfully INFO:    init done: INFO:    platform clock 400000000 INFO:    DDR PLL1 1600000000 INFO:    DDR PLL2 0 NOTICE:  Using static DDR settings NOTICE:  PORSR1: 207f7fff NOTICE:  PORSR2: cf000000 NOTICE:  CLKCCSR: 0 NOTICE:  CL1KCGHWACSR: 30000000 NOTICE:  CL2KCGHWACSR: 8000000 NOTICE:  PLLC1GSR: 18 NOTICE:  PLLC2GSR: 18 NOTICE:  CLKPCSR: 0 NOTICE:  PLLPGSR: 8 NOTICE:  PLLDGSR: 80020 INFO:    Time before programming controller 30 ms INFO:    Program controller registers WARNING: Warning: Optimal CPO value not set. INFO:    total size 4 GB INFO:    Need to wait up to 2680 ms INFO:    Reading debug[9] as 0x10101010 INFO:    Reading debug[10] as 0x10101010 INFO:    cpo_min 0x10 INFO:    cpo_max 0x10 INFO:    debug[28] 0x70006f WARNING: Warning: A009942 requires setting cpo_sample to 0x37 ERROR:   Found training error(s): 0x3002 INFO:    *0x1080000 = 0xff INFO:    *0x1080008 = 0x100013f INFO:    *0x1080010 = 0x140017f INFO:    *0x1080018 = 0x18001bf INFO:    *0x1080080 = 0x80010512 INFO:    *0x1080084 = 0x202 INFO:    *0x1080088 = 0x202 INFO:    *0x108008c = 0x202 INFO:    *0x1080100 = 0x1161000 INFO:    *0x1080104 = 0xff550018 INFO:    *0x1080108 = 0xbab40c52 INFO:    *0x108010c = 0x48d11c INFO:    *0x1080110 = 0xc52c0000 INFO:    *0x1080114 = 0x401020 INFO:    *0x1080118 = 0x1010210 INFO:    *0x1080120 = 0x600041f INFO:    *0x1080124 = 0x18600618 INFO:    *0x1080128 = 0xdeadbeef INFO:    *0x1080130 = 0x2800000 INFO:    *0x1080160 = 0xd501 INFO:    *0x1080164 = 0x3401400 INFO:    *0x108016c = 0x23340000 INFO:    *0x1080170 = 0x8a090705 INFO:    *0x1080174 = 0xc6750606 INFO:    *0x1080190 = 0x606060b INFO:    *0x1080194 = 0xb0c0c00 INFO:    *0x1080220 = 0x701 INFO:    *0x1080224 = 0x4800000 INFO:    *0x1080250 = 0x2116600 INFO:    *0x1080270 = 0xffff INFO:    *0x1080280 = 0xffffff77 INFO:    *0x1080284 = 0xffffff77 INFO:    *0x1080288 = 0x88888800 INFO:    *0x108028c = 0xffffffff INFO:    *0x1080290 = 0x1 INFO:    *0x10802a0 = 0x1 INFO:    *0x1080400 = 0x32c57554 INFO:    *0x1080404 = 0xd4bb0bd4 INFO:    *0x1080408 = 0x2ec2f554 INFO:    *0x108040c = 0xd8000000 INFO:    *0x1080b20 = 0x8080 INFO:    *0x1080b24 = 0x80000000 INFO:    *0x1080b28 = 0x80040000 INFO:    *0x1080b2c = 0x81 INFO:    *0x1080bf8 = 0x20502 INFO:    *0x1080bfc = 0x100 INFO:    *0x1080e40 = 0x80 INFO:    *0x1080f04 = 0x3002 INFO:    *0x1080f08 = 0xe INFO:    *0x1080f0c = 0x14000c20 INFO:    *0x1080f24 = 0x10101010 INFO:    *0x1080f28 = 0x10101010 INFO:    *0x1080f2c = 0x10101010 INFO:    *0x1080f30 = 0x10101010 INFO:    *0x1080f34 = 0x10103000 INFO:    *0x1080f48 = 0x1 INFO:    *0x1080f4c = 0x94000000 INFO:    *0x1080f50 = 0xd000c00 INFO:    *0x1080f54 = 0xb000b00 INFO:    *0x1080f58 = 0x16001600 INFO:    *0x1080f5c = 0x18001800 INFO:    *0x1080f60 = 0xc000000 INFO:    *0x1080f64 = 0x9000 INFO:    *0x1080f68 = 0x20 INFO:    *0x1080f70 = 0x70006f INFO:    *0x1080f94 = 0x80000000 INFO:    *0x1080fb0 = 0x3 INFO:    *0x1080fb4 = 0x1f1f1f1f INFO:    *0x1080fb8 = 0x1f1f1f1f INFO:    *0x1080fbc = 0x1f1f1f1f INFO:    *0x1080fc0 = 0x1f1f1f1f INFO:    *0x1080fc4 = 0x1f1f1f1f INFO:    *0x1080fc8 = 0x1f1f1f1f INFO:    *0x1080fcc = 0x1f1f1f1f INFO:    *0x1080fd0 = 0x1f1f1f1f INFO:    *0x1080fd4 = 0x1f1f1f1f INFO:    *0x1080fd8 = 0x1f1f1f1f INFO:    *0x1080fdc = 0x1f1f1f1f INFO:    *0x1080fe0 = 0x1f1f1f1f INFO:    *0x1080fe4 = 0x1f1f1f1f INFO:    *0x1080fe8 = 0x1f1f1f1f INFO:    *0x1080fec = 0x1f1f1f1f INFO:    *0x1080ff0 = 0x1f1f1f1f INFO:    *0x1080ff4 = 0x1f1f1f1f INFO:    *0x1080ff8 = 0x1f1f1f1f INFO:    *0x1080ffc = 0x1f001f18 ERROR:   Writing DDR register(s) failed ERROR:   Programing DDRC error ERROR:   DDR init failed. NOTICE:  Incorrect DRAM0 size is defined in platfor_def.h ERROR:   mmap_add_region_check() failed. error -22 ERROR:   mmap_add_region_check() failed. error -22 NOTICE:  BL2: v1.5(debug):LSDK-19.09-update-311219-dirty NOTICE:  BL2: Built : 13:08:45, Jul 27 2021 INFO:    Configuring TrustZone Controller INFO:    Value of region base = 7fdffffb INFO:    Value of region base = 7ffffffb INFO:    Value of region base = fbdffffb INFO:    BL2: Doing platform setup INFO:    BL2: Loading image id 3 ERROR:   SD read error - DMA error = 10000000 ERROR:   Read error = fffffffb WARNING: Failed to obtain reference to image id=3 (-2) ERROR:   BL2: Failed to load image (-2) Authentication failure  | 
Solved! Go to Solution.
We have solved this issue. The cause was a combination of two factors:
1. QCVS by default generates a DQ swizzling/remapping pattern in the dq_map registers. We don't have any swizzling on the board, so we had to set dq_map[0..3] to 0 to set a 1:1 bit mapping. There is another thread about this here: https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR4-Memory-Validation-Error-Message/m-p/606956
2. According to erratum A007864 there are problems running 16-bit data widths above 1333 MT/s. We have a 32-bit data width (2x ICs with 16 bits per IC) and it seems this also meets the criteria of A007864, as DDRv failed until we reduced the bus speed to 1300 MT/s.
I am curious why QCVS by default generates such strange DQ remapping values.
We have solved this issue. The cause was a combination of two factors:
1. QCVS by default generates a DQ swizzling/remapping pattern in the dq_map registers. We don't have any swizzling on the board, so we had to set dq_map[0..3] to 0 to set a 1:1 bit mapping. There is another thread about this here: https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR4-Memory-Validation-Error-Message/m-p/606956
2. According to erratum A007864 there are problems running 16-bit data widths above 1333 MT/s. We have a 32-bit data width (2x ICs with 16 bits per IC) and it seems this also meets the criteria of A007864, as DDRv failed until we reduced the bus speed to 1300 MT/s.
I am curious why QCVS by default generates such strange DQ remapping values.
We meet the same problem as we use MT40A1G8SA:062E,but I can't find the erratum A007864 as you refered in before replies, may you provide the erratum A007864 to me, Thanks!
Hi @zhangthink,
The errata can be found in the Documentation section for your SoC. I can't provide the document because NXP now requires an NDA and the document requires a Sharepoint invitation. I'm not positive but I believe this is a new policy and the document used to be publicly available...
If you need an NDA / invitation you will need to contact NXP, either here or via your silicon supplier.
Regards
Hello,
My original NXP account seems to have been deleted, so I am replying under a newly-created account with a different username.
I don't have the CodeWarrior project for this board anymore, but I can provide you with the generated ddr_init.c file which is compiled into ATF. I have attached the file to this post. The file contains the DDR controller registers in the ddr_cfg_regs structure.
In addition, we changed the MEM_PLL_RAT field (DDR clock) in the .rcw file to 13 (meaning 13 * SYSCLK, yielding 1300 MHz assuming SYSCLK is 100 MHz).
Please double-check the other DDR controller settings in this file for compatibility with your board. I hope this helps!
Best regards,
David Norris