Code example and DTS configuration for IRQ5 signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code example and DTS configuration for IRQ5 signal

ソリューションへジャンプ
2,848件の閲覧回数
lucroy
Contributor III

Currenlty working with the LS1021 and looking for a code example and DTS configuration to trigger an interrupt service routine from IRQ5 signal or any of the six available IRQ signals. 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,727件の閲覧回数
lucroy
Contributor III

Found IRQ10 in lsdk1906 but not in the files provided. However pcf2129 was found in the files provided

Thank you

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,728件の閲覧回数
lucroy
Contributor III

Found IRQ10 in lsdk1906 but not in the files provided. However pcf2129 was found in the files provided

Thank you

0 件の賞賛
返信
2,727件の閲覧回数
Pavel
NXP Employee
NXP Employee

See attached files.

These file are .dts file from LSDK 1906 for the LS1088ARDB board.

Find IRQ10 in the fsl-ls1088a-rdb.dts file.

The LS1088ARDB board uses interrupt from the PCF2129.

 

NXP Linux BSP supports sysfs possibility for GPIO interrupt using. Use this possibility for your application.

 

Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信