Code example and DTS configuration for IRQ5 signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code example and DTS configuration for IRQ5 signal

Jump to solution
2,896 Views
lucroy
Contributor III

Currenlty working with the LS1021 and looking for a code example and DTS configuration to trigger an interrupt service routine from IRQ5 signal or any of the six available IRQ signals. 

Labels (1)
0 Kudos
Reply
1 Solution
2,775 Views
lucroy
Contributor III

Found IRQ10 in lsdk1906 but not in the files provided. However pcf2129 was found in the files provided

Thank you

View solution in original post

0 Kudos
Reply
2 Replies
2,776 Views
lucroy
Contributor III

Found IRQ10 in lsdk1906 but not in the files provided. However pcf2129 was found in the files provided

Thank you

0 Kudos
Reply
2,775 Views
Pavel
NXP Employee
NXP Employee

See attached files.

These file are .dts file from LSDK 1906 for the LS1088ARDB board.

Find IRQ10 in the fsl-ls1088a-rdb.dts file.

The LS1088ARDB board uses interrupt from the PCF2129.

 

NXP Linux BSP supports sysfs possibility for GPIO interrupt using. Use this possibility for your application.

 

Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply