secondary USB bootloader example on LPCXpresso 1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

secondary USB bootloader example on LPCXpresso 1769

1,065件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gordon on Tue Feb 22 01:43:54 MST 2011
Hello,

I am wondering if there is any example code for USB bootloader on LPCXpresso 1769. So far, I have only found some code intended for Keil which I am not able to compile in LPCXpresso. Any suggestions on this please?
0 件の賞賛
返信
2 返答(返信)

908件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gordon on Tue Feb 22 03:01:37 MST 2011
Thanks, it seems the problem is solved.
0 件の賞賛
返信

908件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Feb 22 02:31:44 MST 2011
The RDB1768cmsis examples, supplied with LPCXpresso, contains a usb_bootloader example. This will require a minimal amount of porting to LPCXpresso (LPC1768 is the same as a LPC1769 but with a slower maximum clock speed).
0 件の賞賛
返信