problem with debug and pwm in pio1_3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

problem with debug and pwm in pio1_3

765 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Tue Apr 06 18:33:04 MST 2010
Hi, I configured with LPC1114 a example like pio1_3 in pwm output mode, I forget that is a SWIO, when I try to debug other exercise show me a error like this

[IMG]http://img697.imageshack.us/img697/9770/errorlpc.png[/IMG]

LPCXpresso Debug Driver v2.0 (Jan 23 2010 11:18:57)
Looked for chip XML file in C:/nxp/lpcxpresso_3.2/bin/LPC1114/301.xml
Looked for vendor directory XML file in C:/nxp/lpcxpresso_3.2/bin/nxp_directory.xml
Found generic directory XML file in C:/nxp/lpcxpresso_3.2/bin/crt_directory.xml
02: Failed on connect: Ee(02). Not connected to emulator.
Emu(0): Connected. Was: None. DpID: EDB6. Info=T1S6RGRIA
what can I do? best regards
0 项奖励
回复
2 回复数

758 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Tue Apr 06 22:17:23 MST 2010
Hi, finally I resolve this problem, just I put the pin PIO0_1 to ground, and press debug other project, automatically could reprogram and debug, best regards
0 项奖励
回复

758 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Tue Apr 06 21:57:38 MST 2010
Hi I read the note
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/44

I try to do with the vector put to true, but still error, now I try to read something about the isp, but I am very newbie in this microcontroller and the market nxp, any know a guide step by step for reprogramming the microcontroller in the way isp?? sorry for my bad english
0 项奖励
回复