declaring variable at absolute ram location in lpcxpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

declaring variable at absolute ram location in lpcxpresso

512 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by badri89 on Wed Sep 05 22:15:56 MST 2012
Hi all,

I need to define a variable at absolute ram location. I tried the way discussed in this following:

http://support.code-red-tech.com/CodeRedWiki/OwnLinkScripts

But I am getting errors, stating the linkerscript is not found. Though I given the location properly, still it shows the error.

Kindly post the steps involved in  defining variable at absolute ram address. Is there any way without using linkerscripts, like __at attribute in keil?

Thanks
0 项奖励
回复
1 回复

476 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Thu Sep 06 17:17:25 MST 2012
There is a way for doing that in Flash, so it might be the same procedure in RAM:

GPIO_T * myVar= (GPIO_T *)(0xE0028000);


Where GPIO_T is a struct that holds the registers used by GPIO in the LPC2129 uC, but you can use whatever makes sense for your project.

This other snippet is used with LPCXpresso, and works great, although more obscure, 'cause a lot of #define(s) involved:

LPC_TIMER_T * tmr32b1 = (LPC_TMR_TypeDef *)(LPC_CT32B1_BASE);
0 项奖励
回复