debuging and blue screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

debuging and blue screen

2,510 Views
maciek001
Contributor I

Hi! I have problem with LPCxpresso and MCUXpresso. I have lpcxpresso 1347 board. When I try to debug project my PC have blue screen. Probably I have problem with drivers. Wind 7 professional 64-bit SP1. Any solutions?

Tags (2)
0 Kudos
Reply
4 Replies

2,198 Views
lpcxpresso_supp
NXP Employee
NXP Employee

So you appear to be using the GUI flash programmer, rather than debugging. Does debugging, using the Quickstart Panel debug button work correctly?

To be honest, I'm still not sure what else to suggest. It might be worth booting your probe manually and then using the command line GUI flash programmer and seeing if you get any more error information:

Booting LPC-Link 

[Also check out the troubleshooting section of the above FAQ]

https://community.nxp.com/message/630785 

Regards,

LPCXpresso Support

0 Kudos
Reply

2,198 Views
maciek001
Contributor I

It's a miracle. My debuger is running propertly now. I Run another debug probe (LPCXpresso with LPC11U14) and it was run correctly. Next I run previous board (LPC1347). I have no problem! Thanks for your interest in my problem.

0 Kudos
Reply

2,198 Views
lpcxpresso_supp
NXP Employee
NXP Employee

I am afraid that we are not aware of any issues of this form. Thus I'm not sure what we can suggest to help. But at what point do you actually encounter the bluescreen? For instance, can you manually boot the LPC-Link(1) debug probe successfully?

https://community.nxp.com/message/630541 

Regards,

LPCXpresso Support

0 Kudos
Reply

2,198 Views
maciek001
Contributor I

Dear Support,

No bluescreen -> https://www.youtube.com/watch?v=vMKmWdgHD1Q

With bluescreen -> https://www.youtube.com/watch?v=ixwXr8sWNbI

2017-04-25 15:52 GMT+02:00 lpcxpresso_support <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: debuging and blue screen

reply from LPCX support

<https://community.nxp.com/people/lpcxpresso_support?et=watches.email.thread>

in LPCXpresso IDE - View the full discussion

<https://community.nxp.com/message/899838?commentID=899838&et=watches.email.thread#comment-899838>

0 Kudos
Reply