USB connection issue LPC1769

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB connection issue LPC1769

2,126 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Mon Oct 06 11:42:08 MST 2014
Hello everyone,
I tried to start working with my LPC1769, but i have problems with connection. My pc doesn't see it as a drive and cannot install drivers. In addition when i connect LPC1769 to pc red LED2 is blinking all the time. when i try to install mbedWinSerial16466 is says: "the driver could not be installed. No mbed Microcontrollers were found.". What may fix that problem?
0 Kudos
Reply
5 Replies

1,915 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Oct 06 13:50:40 MST 2014
The LPCXpresso board that you have cannot be used directly from mbed. You can use mbed to create an application that will run on this board, but mbed cannot download the application to this board - you will need to use LPCXpresso IDE.

Alternatively, you should purchase a board that does support the mbed download interface. There are many such boards on the mbed website.
0 Kudos
Reply

1,915 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Mon Oct 06 13:40:11 MST 2014
Problem may occur because of connecting cable? Maybe i should check new one, i don't have any other devices that use Mini-B cable, so i don't know if it works properly.
0 Kudos
Reply

1,915 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Oct 06 12:19:33 MST 2014
This picture shows a 'LPCXpresso 1768' board...

If you install LPCXpresso before you connect it, all drivers are installed  :)

See: http://www.lpcware.com/lpcxpresso
0 Kudos
Reply

1,915 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Mon Oct 06 12:11:10 MST 2014
It looks like http://mbed.org/media/uploads/nxpfan/lpcxpresso1768.jpg
when i connect it via USB, PC tries to install drivers, but fails. Maybe i tried to install mbed without a reason :) It's my first time with ARM microcontrollers so I'm a bit confused. What should i do to connect properly that microcontroller and run simple Blink program for example, in LPCXpresso?
0 Kudos
Reply

1,915 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Oct 06 11:57:53 MST 2014

Quote: Zahoq
...my LPC1769, but i have problems with connection.



:quest:  Is it a single LPC1769 or a board, too  :quest:


Quote: Zahoq
My pc doesn't see it as a drive and cannot install drivers.



Which software is your LPC executing?


Quote: Zahoq
... i try to install mbedWinSerial16466 is says: "the driver could not be installed. No mbed Microcontrollers were found.". What may fix that problem?



Could be useful if you explain what you are trying to connect as MBED...
0 Kudos
Reply