Target reported error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Target reported error

6,052 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpc1857 on Mon Jan 07 02:19:20 MST 2013
Hi,

When i debug my code in LPCXpresso v4.3.0 then after downloading image it shows the error like


Quote:

  15: Target error from Set break/watch
  Unable to set an execution break - no resource available.



I have not set any breakpoint in my code.check the solution on net but not luck:confused:.

Please help.
0 项奖励
回复
3 回复数

4,934 次查看
Gretsch
Contributor II

Took me a while to figure this one out...

In my case it was because a breakpoint that I had set was no longer in a valid line of code.

This is a terrible bug.  Just because a breakpoint can't be set, the whole debugger should not fall flat on its face.

Invalid breakpoints should be simply ignored skipped over on failure.  Every other (good) debugger in the world *silently* ignores invalid breakpoints.  

Devs all know they need to clean up old breakpoints periodically, but don't *force* me to do it.

5,890 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Mon Jan 07 02:36:58 MST 2013
Be useful if you told us what MCU you were debugging!

Also, have you read this FAQ - How many breakpoints or watchpoints can I set?
http://support.code-red-tech.com/CodeRedWiki/HowManyBreakpoints

HTH!

5,890 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by modestt on Mon Jan 07 02:32:05 MST 2013
could you share your hardware connections setup etc ?
0 项奖励
回复