Target reported error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Target reported error

6,187件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpc1857 on Mon Jan 07 02:19:20 MST 2013
Hi,

When i debug my code in LPCXpresso v4.3.0 then after downloading image it shows the error like


Quote:

  15: Target error from Set break/watch
  Unable to set an execution break - no resource available.



I have not set any breakpoint in my code.check the solution on net but not luck:confused:.

Please help.
0 件の賞賛
返信
3 返答(返信)

5,069件の閲覧回数
Gretsch
Contributor II

Took me a while to figure this one out...

In my case it was because a breakpoint that I had set was no longer in a valid line of code.

This is a terrible bug.  Just because a breakpoint can't be set, the whole debugger should not fall flat on its face.

Invalid breakpoints should be simply ignored skipped over on failure.  Every other (good) debugger in the world *silently* ignores invalid breakpoints.  

Devs all know they need to clean up old breakpoints periodically, but don't *force* me to do it.

6,025件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Mon Jan 07 02:36:58 MST 2013
Be useful if you told us what MCU you were debugging!

Also, have you read this FAQ - How many breakpoints or watchpoints can I set?
http://support.code-red-tech.com/CodeRedWiki/HowManyBreakpoints

HTH!

6,025件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by modestt on Mon Jan 07 02:32:05 MST 2013
could you share your hardware connections setup etc ?
0 件の賞賛
返信