LPCXpresso Using ISP Uart Flash Program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso Using ISP Uart Flash Program

2,020件の閲覧回数
mrcbis
Contributor I

Hello,

I am just starting using LPCXpresso IDE under Ubuntu 16.04LTS. I wonder if there is any way to program OnChip flash memory using ISP Uart BootLoader mode of the device. I am able to communicate with the chip using lpctools but I wonder if there is some way to integrate the flash programming phase inside the LPCXpresso IDE. I have a custom board and I have no jtag connection available. The only way to program the flash memory is using a Uart cable to download image to the device (using an USB -> Uart adapter that is working with lpctools).

Regards

Marco Bisio

ラベル(3)
0 件の賞賛
返信
1 返信

1,569件の閲覧回数
converse
Senior Contributor V

Nothing in the ide, but try mxli: mxli - Marc's exquisite LPC ISP tool 

0 件の賞賛
返信