LPC1114 uart and GPIO debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1114 uart and GPIO debugger

626件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kalyani on Fri Dec 03 21:37:55 MST 2010
HI,
   I am using lpc1114 lpcxpresso board. when i am using the debugger, when i configure
the UART LCR register the peripheral window of uart shows that the UART RBR register is being updated.

Incase of the IO configuration for port 0.4, the bits used for mode setting are 8 and 9, where as the debugger shows the mode setting bits are 3 and 4.
0 件の賞賛
返信
1 返信

607件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Dec 06 04:56:17 MST 2010
Thank you for reporting these issues with the peripheral viewer. We will investigate with a view to fixing in a future release of the LPCXpresso IDE.

Regards,
CodeRedSupport
0 件の賞賛
返信