LPC1114 uart and GPIO debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1114 uart and GPIO debugger

600 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kalyani on Fri Dec 03 21:37:55 MST 2010
HI,
   I am using lpc1114 lpcxpresso board. when i am using the debugger, when i configure
the UART LCR register the peripheral window of uart shows that the UART RBR register is being updated.

Incase of the IO configuration for port 0.4, the bits used for mode setting are 8 and 9, where as the debugger shows the mode setting bits are 3 and 4.
0 Kudos
Reply
1 Reply

581 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Dec 06 04:56:17 MST 2010
Thank you for reporting these issues with the peripheral viewer. We will investigate with a view to fixing in a future release of the LPCXpresso IDE.

Regards,
CodeRedSupport
0 Kudos
Reply